Pack Workbench

Use this form to group pick lists together into a shipment. This form is not a required part of the process. If a shipment is going to be built off of a single pick list, you do not need to use this form; however it can still be used. Users can be assigned to pack the items, and the location that the goods should be moved to after packing can also be assigned. This form also shows other orders or pick lists for the customer in question for a selected pick list. This allows you to decide if you should wait on packing the pick list in question so that you can create a combined shipment at a later time.

Orders Tab

The orders tab shows customer orders for the customer of the pick list line selected in the pick list grid. You can view any upcoming orders that may be picked so they can be grouped together if you wish. The fields in the grids on this tab are all read-only.

Pick Lists Tab

This tab shows other pick lists for the customer of the selected pick lists, with a status of opened. You can view any pick lists that have yet to be picked so they can be grouped together if you wish. All of the fields on this tab are read-only.

 


Related Topics

Picking, Packing, and Shipping Overview

Grouping Pick Lists into a Shipment