Shipment Master

Use the shipment master form to create, update, and maintain a shipment.

The Packages tab shows packages that have been created for the shipment. All of the fields on this tab are read-only. The tracking number that displays is the lead tracking number. For example, if three packages are listed, all of them display the same tracking number. That tracking number is the number for the first package.

The Pick Lists tab shows the details of which Order/Line/Release quantities are being fulfilled by the shipment and which lots are being used. It also lists the pick lists that the line/releases came from and shows the current location where the items reside. After shipping, the quantity shipped is updated and viewable here.  All of the fields on this tab are display-only.


Related Topics

Picking, Packing, and Shipping Overview

Shipping a Shipment