Note: If you want to print packing slips for shipments added to delivery orders, use the Print Delivery Order Packing Slip Report.
The Packing Slip Selection and Pre-Ship Packing Selection forms are similar in appearance and function. The purpose of both forms is to allow you to specify which customer orders to have packing slips printed for. Both forms display the orders and lines that are available for packing and that meet the selection criteria specified on the Packing Slip form.
Both forms are accessed from the Packing Slip form. The system opens the
After selecting the report type, to open the appropriate form, click Process.
The Shipping tab displays the shipment records for the current lines or releases selected on the General tab. You must select enough quantity to match the target quantity.
TIP: You can select or deselect all orders with the Select All or Deselect All options on the Actions menu.