Buyer Home - Tasks Tab
The Tasks tab contains three sections:
- Alerts: The buttons in this section
have red numbers if the number is above zero. The number is green
if it is zero. If you click the Overdue Lines button, the Purchase
Order Lines form opens. If the number on the button is red, the
Purchase Order Lines form displays the number of regular PO
lines (the red number on the button) that are overdue as of "today"
that have a PO and PO line status of ordered and the quantity received
is less than the quantity ordered for a specific buyer. If you click
the Overdue Releases button, that opens the Purchase Order
Blanket Releases form. If the number on the button is red, the
Purchase Order Blanket Releases form displays the number of
blanket PO releases that are overdue as of "today" (the
red number on the button) that have a PO and PO release status of
ordered and the quantity received is less than quantity ordered for
a specific buyer.
- Tasks: The tasks section lists
the tasks assigned to the logged-in user. See Adding
and Viewing User Tasks for more information about tasks.
- Inbox: The Inbox section lists
the messages for the logged-in user. See the Inbox
form for more information about the inbox. Double-click a field in
the Inbox grid to view all emails that share that value. All Inbox
fields can be filtered with the exception of Read and Expired.
EXAMPLE: To view only the emails
from John Doe, double-click John Doe in the From field.