Example - Advance Ship Notice Calculations
The following information explains the calculations
the system uses for the COD amount and the total charges amount.
The following are fields on the Cost Info tab
of the Advance
Ship Notices form:
- Freight Charges - Enter the freight
charges for this transfer order.
- Freight Method - Are freight
charges prepaid or collected on delivery?
- COD Method - Are COD fee charges
prepaid or collected on delivery?
- COD Amount - Enter the amount
to collect on delivery.
- COD Fee - Enter the fee charged
for delivering COD.
- Total Charges - Enter total charges
for this transfer order.
NOTE: Freight charges
are initially equal to the freight amount from the CO header from which
the ASN was created. When the sum of the ASN item's rates are less than
or greater than zero, the system resets this value to the total of the
ASN item's rates.
The system sets the default value of the COD Amount as the SUM
of the following two values:
- If Freight Method is Collect, then include the freight
charges; otherwise, 0 (zero)
- If COD Method is Collect, then include the COD fee;
otherwise, 0 (zero)
The system calculates the Total Charges as follows:
- If Freight Method is Prepaid and:
- COD Method is Prepaid,
the system uses COD Amount.
- COD Method is Collect,
the system uses the greater of COD Amount or COD Fee.
- If Freight Method is Collect and:
- COD Method is Prepaid,
the system uses the greater of COD Amount or COD Fee.
- COD Method is Collect,
the system uses the greater of COD Amount or (Freight
+ COD Fee).
Related Topics