Goods Receving Notes Overview

Use the Goods Receiving Notes (GRN) functionality to link a receipt to multiple purchase orders for the same vendor. GRNs can be created manually or automatically from an EDI ASN.

A GRN has one of four statuses:

Create a GRN

GRNs are created in one of the following ways:

Create GRN Lines

GRN lines are created in one of the following ways:

GRN Report

Use the Goods Receiving Note Report form to print a report which shows GRN status and line information. Select from a range of GRNs and vendors.

Change GRN Status

Use the Change Goods Receiving Note Status utility to change the status of a GRN. You can change from one status to another status in the following cases:

Delete a GRN

GRNs with a status of In Process or History can be deleted. Use the Delete Goods Receiving Note utility to delete a range of GRNs. You can delete GRNs individually without using the Delete Goods Receiving Note utility. On the Goods Receiving Notes form, click the delete button in the toolbar to delete the current GRN.


Related Topics

Change Goods Receiving Note Status

Delete Goods Receiving Notes

Generate Goods Receiving Note Lines

Goods Receiving Note Report

Goods Receiving Notes

Goods Receiving Notes Lines