Point of Sale Overview
You can use the forms in the Point of Sale (POS) module to handle walk-in
customer transactions such as customer sales orders, service orders, returns,
or rentals. POS includes a logical “cash drawer” that the cashier accesses
by logging in and out. Separate drawers are maintained for customer orders
vs. service orders. The cashier specifies the amount in the drawer when
the drawer is checked out and again during end-of-day processing. The
balance in the drawer, taking into account all transactions that occurred,
must be reconciled when the drawer is checked in. If the drawer is out
of balance, an adjustment transaction is created.
POS transactions for new sales are posted to Accounts Receivable as
the sale occurs. Balance adjustment transactions, if needed, are posted
during End of Day processing.
NOTE: The POS module
is not intended to be used with external AR financials. If the Use
External A/R System option is selected on the External
Financial Interface Parameters form, do not use the POS module.
Because POS transactions are normally walk-in sales, the POS module
supports transactions only using your domestic currency.
These forms are included in base SyteLine
and do not require any separate licensing:
- POS Setup: Use this form
to set up parameters that are used during Point of Sale transactions.
You define the cash drawers here, and cashiers use the Checkout button
to exclusively check out a drawer.
- Point of Sale Entry: This
is the main form used for POS customer order or service order transactions.
The Login button opens the POS Logon
form, where users log into the cash drawer. From the Point of Sale
Entry form, you can open these modal forms as needed:
- POS Material, Point of Sale
Labor, POS Miscellaneous Charge, and POS Payment:
These are modal forms that are opened from buttons on the Point of Sale Entry form, so
you can enter information about the items, labor, amounts, and
payments included in the order.
- POS Customer Orders:
Use this modal form to handle a later customer pickup of an item
that was already sold.
- POS Reverse Lookup Option:
Use this modal form to look up and reverse charges during a customer
return of materials from a POS order.
- POS Inquiry: Use this form
to look up information about past POS orders.
- POS Checkout/Checkin: Licensed
SyteLine Service users
who use service contracts to rent out equipment can use this form
to check out and check in rental equipment, and to collect the appropriate
rental amount from the renter. Use the Checkout/Checkin button
on the Contracts form to open this form.
- POS End of Day Processing:
Use this utility reconcile the cash that remains in the cash drawer
with the POS transactions that occurred during the day, and to perform
any required balance adjustment before you check in the drawer.
Related Topics
Setting up the Point of Sale
(POS) Feature
Processing Orders with Point of
Sale
Processing Rentals
with Point of Sale
Processing Returns with Point
of Sale
Handling Walk Up-Sales
with Point of Sale