Copying Orders and Estimates
Use the Copy 
 Orders and Estimates form to copy information from estimates or 
 orders to other estimates or orders.
About the Copy Process
The following conditions exist for using the Copy 
 Orders and Estimates activity:
	- In general, these types of information are not copied: 
	
		- Historical information that is specific to the original order 
		 and that does not apply to new orders, for example, accumulated 
		 values, effective date, and expiration date..
- Calculated values such as sales tax that will be recalculated 
		 based on which lines are copied.
 
- When you copy from an estimate to an order, the system extracts 
	 the freight tax code and miscellaneous tax code fields from the corresponding 
	 fields on the Tax Systems form. When you copy an order to an order, 
	 however, the system copies the freight tax code and miscellaneous 
	 tax code fields from the order.
- When you copy from an estimate to an order, the system extracts 
	 the transaction nature, delivery terms, and process indicator fields 
	 from the Customers form. When you copy an order to an order, however, 
	 the system copies these fields from the order.
- When you copy from an estimate to an order, the system extracts 
	 the origin and commodity code fields from the item on the estimate. 
	 When you copy from an order to an order, however, the system copies 
	 these fields from the order.
- When you copy from an estimate, the system does not copy the non-inventory 
	 line items.
- If you copy blanket customer orders, the system does not copy the 
	 attached releases.
- When you copy a customer order, the system does not copy the value 
	 for Promotion 
	 Code, if one is specified.
- When you copy an estimate to a regular order, the system does not 
	 copy the Cust Quote field on the estimate to the Cust PO field on 
	 the regular order. When you copy from an estimate to another estimate, 
	 however, the Cust Quote field is copied.
- When you copy orders or estimates that contain commission distributions 
	 to a new order or estimate, the system copies those distributions 
	 to the new order or estimate. When you copy an order or estimate to 
	 another (already existing) order or estimate, the commission distribution 
	 records are not copied.
- When you copy orders and estimates that contain order level discounts, 
	 the system also copies those discounts.
- When you copy orders or estimates that include a kit, 
	 the value of the Print Kit Components on Customer Paperwork field 
	 is also copied. When copying an order to an order, this value comes 
	 from the original order. When copying an estimate to an order, this 
	 value comes from the Items form.
- When an order at the originating site is copied, the system also 
	 copies the lines to the other order. If these lines are for different 
	 shipping sites, the system connects to each shipping site and places 
	 the order header and order lines at each site. The system creates 
	 a copy of this order at the originating site. When estimates are copied, 
	 the site copying the order becomes the default originating site. The 
	 shipping site on each line also fills in with the name of the current 
	 site. If an order is copied by a site that is different than the originating 
	 site on the copied order header, the site that is copying the order 
	 becomes the originating site on the new order.
- The Taken By field defaults to the current user's initials.
NOTE: You cannot 
 copy a regular customer order or estimate to a blanket order.
CAUTION: When 
 you copy an estimate to an order for a customer that requires a letter 
 of credit number, a warning message displays. Also, if you copy one customer 
 order to another, any existing letter of credit number is not copied to 
 the new customer order.
To Copy Orders and Estimates
	- In the From, field, specify the 
	 source or accept the default, Estimate Order. Options include: 
	 
	
		- Estimate Order
- Customer Order
- Blanket Order
- History Order
 
- Based on your From selection, specify one of these values: 
	
		- Estimate Number - If you 
		 select Estimate Order, the system prompts you for a valid 
		 estimate order number.
- Order Number - If you select 
		 Customer Order, the system prompts you for a valid customer 
		 order number.
- Blanket Number - If you select 
		 Blanket Order, the system prompts you for a valid blanket 
		 order number.
- History Number - If you select 
		 History, the system prompts you for a valid history order 
		 number.
 
- In the Starting and Ending 
	 Line Numberfields, specify the first and last line numbers to 
	 copy, or accept the default from the order.
- In the To field, specify the 
	 destination to which this estimate is to be copied. Destination options 
	 include: 
	
		- Customer Order (default value)
- Estimate Order
- Blanket Order
 NOTE: If this 
	 field is left blank, the system creates a new order. 
- In the Option field, specify 
	 one of these options: 
	
		- Insert a Range (default value)
- Replace a Range
- Delete and Then Insert a Range
 
- Click Process.
Related Topics
Estimating Steps