Creating an Estimate
To create quotes for customers detailing the costs
and delivery times of goods or services, use the Estimates
form.
- Select Actions > New.
- Enter the appropriate data. The required fields are:
- Estimate - Enter an estimate
number or accept the system default, which is the next unique
numerical value.
To start all estimates with the same prefix followed by a computer-generated
number, you can set up a global prefix in the Shop
Floor Control Parameters form. However, the prefix and
numerals together can only total ten characters in length.
- Quote Date - Enter the date
on which the quote is effective, or accept the default, which
is the current date.
- Expiration Date - Enter the
date on which the quote will expire, or accept the default, which
is the current system date plus the value of the Std Expiration
Period field on the Shop Floor Control Parameters form.
- Status - Select the status,
or accept the default value, Working.
- Select the Tax Info tab.
- In the Tax Code field, enter the tax code to use in calculating
taxes on the order for Tax System 1.
- (Optional) Enter the appropriate data in these optional fields
on other tabs:
- Customer - Enter the customer
ID.
- Contact - Enter a contact
name or accept the default from the Customers form.
- Cust Quote - Enter a quote
number provided by the customer.
- Terms Code - Enter a valid
payment term code.
- Order Discount - Enter the
order discount amount or percentage agreed to in the quote, if
any.
- Save the form.
Related Topics
Estimating Steps