When two separate software packages transmit data via EDI, their transmission processes must not concurrently access the same data files. For example, synchronization problems occur if SyteLine EDI writes data to a flat file and the translator attempts to read the flat file at the same time. The system uses a lock mechanism to handle this problem.
When EDI needs to write information to a flat file, it first checks to see if a lock file exists.
If you are using a translator other than those listed in the About EDI Translators topic, you must make sure the translator checks for and creates the lock file. This section lists the lock file filenames you must use with your translator. Create the appropriate lock file when writing to or reading from the flat file.
The following table lists the name of the lock file for each transaction for supply-side EDI. Supply-side lock files reside in the supply-side Outbound Data directory.
| TRANSACTION | X12 / EDIFACT | LOCK FILENAME |
|---|---|---|
| Outbound Planning Schedules | 830 / DELFOR | 830_LOCK |
| Outbound Purchase Orders | 850 / ORDERS | 850_LOCK |
| Outbound Shipping Schedules | 862 / DELJIT | 862_LOCK |
| Inbound PO Acknowledgment | 855 / ORDRSP | 855_LOCK |
| Inbound Vendor Advanced Ship Notice | 856 / DESADV | 856_LOCK |
| Inbound Vendor Invoice | 810 / INVOIC | 810_LOCK |
The following table lists the name of the Lock file for each transaction for Demand-side EDI. Demand-side lock files reside in the demand-side Outbound Data directory.
| TRANSACTION | X12 / EDIFACT | LOCK FILENAME |
|---|---|---|
| Inbound CARaS EDI Ship Transactions | N/A | SHP_LOCK |
| Inbound Planning and Shipping Schedules | 830 / DELFOR & 862 / DELJIT | REQ_LOCK |
| Inbound Purchase Orders | 850 / ORDERS | ORD_LOCK |
| Outbound PO Acknowledgment | 855 / ORDRSP | ACK_LOCK |
| Outbound Advanced Ship Notice | 856 / DESADV | ASN_LOCK |
| Outbound Customer Invoice | 810 / INVOIC | INV_LOCK |
This section describes how EDI processes flat files. Your translator software should use the same logic.
EDI performs these steps when writing data to the flat files:
EDI performs these steps when reading data from the flat files: