Implementing DIFOT (Delivered In Full and On Time)
DIFOT (Delivered In Full and On Time) is a standard used to measure 
 delivery performance in a supply chain.
To implement DIFOT evaluations:
	- Set the default DIFOT criteria. 
	Use the Order Entry Parameters 
	 form, DIFOT tab. These values 
	 become the default values for the system. You can override them at 
	 these levels: 
		- Customer
- Customer order
- Customer order line
- Customer order blanket line
- Customer order blanket release
 To set the maximum: 
		- Percentage of items that can be shipped in excess of 
		 the number ordered and still be considered “in full,” use the 
		 Ordered Qty Tolerance Over field.
- Percentage of items that can be shipped below the number 
		 ordered and still be considered “in full,” use the Ordered 
		 Qty Tolerance Under field.
- Number of days before the due date that an order can 
		 ship and still be considered “on time,” use the Shipped Before 
		 Due Date Tolerance field.
- Number of days after the due date that an order can ship and 
		 still be considered “on time,” use the Shipped 
		 After Due Date Tolerance field.
 
- (For existing customer order records) Use the Update 
	 Order DIFOT Policy form to generate DIFOT data.
- Use the system to create and fill customer orders that generate 
	 DIFOT data.
- Use the Delivered 
	 In Full And On Time Report form to create the desired DIFOT report.
Related Topics
About DIFOT (Delivered 
 In Full and On Time)