Setting Up Shipping Charges for Credit Card Customers
When customer orders are placed with a credit card, the shipping charges 
 must be calculated before the order is submitted, so that customers know 
 the total amount that is to be charged. You can specify a Ship Method 
 for the order, and then the system calculates the shipping freight charges 
 based on that ship method. You can then ship and invoice the customer 
 order either through standard processes, or through the Pick/Pack/Ship 
 process. 
The Ship Method and associated fields and forms are intended for use 
 with the Credit Card Interface. 
Note: Some of this information also applies 
 to credit card orders received from the SyteLine 
 portals; however, that process has some different steps, so  refer 
 to the SyteLine Portals Setup and Administration 
 Guide, section on "Setting Up Shipping Charges for Portal 
 Orders."
To set up shipping charges for credit card orders, follow these steps:
	- On the Freight Charge Methods 
	 form, define methods (rules) that are used to calculate approximate 
	 shipping freight charges. For example, freight can be calculated per 
	 item, by total order weight, using maximum or minimum freight charges 
	 per order, etc. For more information about this form, see Freight 
	 Charge Method Examples or the specific field help.
- On the Ship Methods form, 
	 define shipping methods for credit card orders. For each ship method, 
	 you can specify the freight method to use, and the minimum and maximum 
	 days to ship. (Later, during the order entry process, when you specify 
	 that an order is to be paid by credit card, you specify the Ship Method.) 
	  
- On the Ship Method Groups 
	 form, combine ship methods into groups that can be assigned to customers 
	 who pay by credit card. Each of the ship methods included in the assigned 
	 group is available for selection in the Ship Method list during the 
	 order entry process.
- On the Customers or Multi-Site Customers forms, if a 
	 customer will use a credit card to pay for orders, select a Ship Method 
	 Group for the customer.
- On the Order Entry Parameters 
	 form, specify a default ship method group. This default group determines 
	 the list of ship methods that are displayed for a new credit card 
	 order, if the customer does not have a ship method group defined. 
	 
- Optionally, on the Items 
	 or Multi-Site Items form, 
	 specify a Freight amount that is to be charged for items that require 
	 special freight charges. This amount overrides the default Charge 
	 per Item set on the Freight Charge 
	 Methods form.
- When you enter a credit card order on the Customer 
	 Orders form, when you click Pay 
	 with Credit Card,  you can specify one of the ship methods 
	 defined in step 2. 
	When the freight (shipping) charge is calculated, it is stored in 
	 the Freight field on the Customer Orders form. Entering a ship method is optional. If no method is entered, no 
	 shipping freight charges are calculated for the order, and the standard 
	 process for specifying freight should be used instead. 
For more information about using each of these forms in this task, review 
 the form and field online help.
Related Topics
Picking, 
 Packing, and Shipping Overview
Freight 
 Charge Method Examples
Shipping 
 and Invoicing Credit Card Orders