Errors That Stop Demand EDI CO Transaction Posting
The following errors may occur when posting EDI customer
orders to SyteLine.
- Credit Limit Exceeded - The EDI
customer order is over the customer's credit limit.
- Cust-PO is Blank - The EDI customer
order does not contain a customer PO number when one was expected.
Verify that the EDI customer order includes a valid customer PO number.
- Invalid Customer - The customer
on the EDI customer order is not a valid customer. Verify that the
customer exists on the EDI order.
- Invalid Item- The item number
on the EDI customer order blanket line is not a valid SyteLine item. Verify
that the item of the EDI order blanket line is a valid SyteLine item.
- Invalid Order Type - The EDI
customer order type is not a valid order type of Regular or Blanket.
Verify the EDI order type.
- Invalid Price Code - An invalid
price code was found on the EDI customer order line or EDI customer
order blanket line.
- Invalid Ship-Via - The ship via
code on the EDI order is invalid.
- Invalid Unit of Measure - The
EDI Customer Order Line/Releaseunit of measure is not valid.
Verify the EDI Order Line/Release contains a valid SyteLine unit of measure.
- Invalid Unit Price- The price
imported on the EDI customer order line/release does not match the
SyteLine
calculated price. Verify which price is correct and make the appropriate
change.
- Item Is Obsolete and Cannot Be Posted
to an Order - There is a blanket line without any releases and
the blanket line item is not found in the item table.
- Not One Item Price Exists- No
pricing is set up in SyteLine
for this item. Add either an item pricing record or a customer-item
cross-reference pricing record for this item.
- Order Already Exists- A SyteLine customer order
already exists for the incoming EDI customer order and the SyteLine order is not
an EDI order.
- Order must be Blanket- The EDI
customer order attempted to update a SyteLine
order that was an EDI order, but was not the specific EDI order type
(BCO/BPO/RPO).
- Unable to Add More Order Line Items-
The EDI customer order attempted to update a SyteLine
order with 9999 or more line/releases. To correct, close the current
order and line, and open a second order and line.
- Unable to Add More Blanket Releases
- The maximum number of blanket releases, 9999, has been reached for
a particular blanket line.
- Warehouse for Item Is Invalid
- The Item-Warehouse record for the item on the EDI customer order
blanket line does not exists. Verify that the item and warehouse of
the EDI order blanket line are valid.
- XRef not Permitted- The EDI customer
order attempted to update a SyteLine
order with a line/release cross-referenced to a job or item. An update
of SyteLine
orders with cross-referenced line/releases is not permitted. Remove
the cross reference.
Related Topics
Electronic
Data Interchange (EDI) Overview
EDI Steps
Errors
That Stop Supply EDI Transaction Posting