Vendor Contract Pricing Setup
To set up the pricing for vendor items:
	- Select the vendor from either the Vendor Contracts form 
	 or the Vendor Contract Prices form. If you are on the Vendor 
	 Contracts form, click Pricing to link to the Vendor Contract 
	 Prices form.
- Select the item to price.
- Status is set to Approved by default. If the new pricing is for 
	 a vendor contract price that is not yet approved, select Pending in 
	 the Status 
	 field. It can be approved later using the Approve button 
	 on this form or using the Change 
	 Vendor Contract Price Status Utility.
- Enter the effective date of the price.
- Enter the landed cost charges: freight, duty, brokerage, insurance, 
	 and local freight.
- You can create up to five price breaks for the item. Enter the 
	 quantity of the price break in the Break 
	 Qty field.
- Enter the unit price. This value is based on the base unit of measure 
	 for the vendor, not the item.
- Repeat these steps for each price break you want to create.
- When you have finished creating the prices, click Save.
Related Topics