Specify the maximum number of vouchers to place within a complete business transaction document. For example, if there are five A/P transaction records, and Maximum Batch Size is set to 2, there will be three XML documents sent:
Setting the batch size to 0 (zero) posts all transactions in the batch as a single XML document.
This field is enabled when Use External A/P System is selected.
For Infor Global Financials (IGF) integration, this setting is not applicable. Use the default value.