Exchange Rate

The exchange rate between the customer's currency and the domestic currency displays. At posting time, if the payment transaction rate is blank, the posting routine will use the current rate.

NOTE: If this is a reapplication of a payment, the original exchange rate is used.

CAUTION: Reducing the number of decimal places in this field may cause rounding problems.