Unit Code (1-4)

Enter or select a unit code for each segment you use.

NOTE: The system is set up to take the departmental unit code (Unit Code 1) and use it in the account default, whenever a particular work center uses a department.

On the Import Journal Entries form, unit codes should be mapped to journal unit codes that are set to Accessible. The following rules apply when using unit codes on this form: