You enter a payment for $150, and then select three $50 vouchers in the grid to apply against that payment.
The grid shows:
| Type | Voucher | Site | PO | Check | Invoice Date | Due Date | Amt to Pay | Discount |
|---|---|---|---|---|---|---|---|---|
| Voucher | 101 | 01 | P000001 | 05/15/2002 | 06/15/2002 | 50.00 | 0.00 | |
| Voucher | 150 | 01 | P000007 | 06/15/2002 | 07/15/2002 | 50.00 | 0.00 | |
| Voucher | 156 | 01 | P000010 | 06/22/2002 | 07/22/2002 | 50.00 | 0.00 |
Selecting Apply creates three distribution records, one for each voucher.
You enter a payment for $100, and select no transactions in the grid. The payment date is 06/15/2002. You save the payment, and then select Apply to apply it. A payment distribution for an open amount of $100 is created. The grid shows:
| Type | Voucher | Site | PO | Check | Invoice Date | Due Date | Amt to Pay | Discount |
|---|---|---|---|---|---|---|---|---|
| Open | 01 | 06/15/2002 | 06/15/2002 | 100.00 | 0.00 |
You enter a payment for $100, select a voucher with an amount less than $100 so that some of the payment amount is left to apply. You save the payment. You then select a voucher for $60 and select Apply. Two payment distributions are created, one with the type Voucher in the amount of $60, and the other with the type Open in the amount of $40. Both the voucher and the open payment are shown as selected in the grid.
| Type | Voucher | Site | PO | Check | Invoice Date | Due Date | Amt to Pay | Discount |
|---|---|---|---|---|---|---|---|---|
| Open (dist) | 01 | 06/15/2002 | 06/15/2002 | 40.00 | 0.00 | |||
| Voucher | 102 | 01 | P000001 | 05/15/2002 | 06/15/2002 | 60.00 | 0.00 |
You enter a payment for $0, and then select a voucher and an open payment.
| Type | Voucher | Site | PO | Check | Invoice Date | Due Date | Amt to Pay | Discount |
|---|---|---|---|---|---|---|---|---|
| Open | 01 | P000001 | 06/15/2002 | 06/15/2002 | 50.00 | 0.00 | ||
| Voucher | 101 | 01 | P000001 | 05/15/2002 | 06/15/2002 | 50.00 | 0.00 |
Selecting Apply automatically posts the open payment. The voucher number in A/P Posted Transactions now says 101. The A/P account in the original A/P Posted Transactions record for the open payment is 11600. The A/P account in the parameters is 20000. Journal entries created are:
| 29 | * 06/15/2002 | 20000 | 50.00 | APPR | 1 |
| Accounts Payable | 50.00 | USD | 1.000 | ||
| 30 | * 06/15/2002 | 11600 | 50.00 | APPR | 1 |
| AP Deposit | 50.00 | USD | 1.000 |
You enter a payment for $75, and then select multiple vouchers and an open payment.
You select two vouchers: voucher 101 with a due date of 06/15/2002 for $50, and voucher 150 with a due date of 07/15/2002, for $75. You then select a $50 open payment with a due date of 06/15/2002. Selecting Apply applies the open payment of $50 to voucher 101 and posts it. A/P Posted Transactions will show the payment with a voucher number of 101. The new payment of $75 is applied to voucher 150, and a payment distribution is created. When the grid in A/P Quick Payment Application is refreshed, it will look like this:
| Type | Voucher | Site | PO | Check | Invoice Date | Due Date | Amt to Pay | Discount |
|---|---|---|---|---|---|---|---|---|
| Voucher | 150 | 01 | P000007 | 06/15/2002 | 07/15/2002 | 75.00 | 0.00 |
No transaction line for voucher payment 101 displays in the grid, because voucher 101 becomes fully paid after you select Apply.
Reapplication of an open payment.
You enter an open payment for reapplication with an amount of $1000. The grid shows a voucher selected for $1000. The system creates the payment distribution when you select Apply. The A/P account in the original A/P Posted Transaction record for the open payment is 11600 (Deposit account). When you apply the open payment, payment application occurs within the due date, so the system automatically enters a discount for $50 in the Discount column. When the payments post through payment posting, the posted journal entries are as follows:
| 55 | * 01/18/2003 | 11600 | 1,000.00 | APPR | 656 |
| AP Deposit | 1,000.00 | USD | 1.000 | ||
| 56 | * 01/18/2003 | 12100 | 50.00 | APPR | 656 |
| Open A/P Account | 50.00 | USD | 1.000 | ||
| 57 | * 01/18/2003 | 20000 | 1,000.00 | APPR | 656 |
| Accounts Payable | 1,000.00 | USD | 1.000 | ||
| 58 | * 01/18/2003 | 50400 | 50.00 | APPR | 656 |
| Purchase Discount and Allowance | 50.00 | USD | 1.000 |
Applying the open payment to the voucher within A/P Quick Payment Application would yield the journal entries shown below. Note that the system creates an Open payment distribution for the remaining $50 of the open payment that was not applied (due to the applied discount). This payment distribution is then posted normally through payment posting.
| 55 | * 01/18/2003 | 20000 | 1,000.00 | APPR | 656 |
| Accounts Payable | 1,000.00 | USD | 1.000 | ||
| 56 | * 01/18/2003 | 50400 | 50.00 | APPR | 656 |
| Purchase Discount and Allowance | 50.00 | USD | 1.000 | ||
| 57 | * 01/18/2003 | 11600 | 950.00 | APPR | 656 |
| AP Deposit | 950.00 | USD | 1.000 |
Reapplying an open payment to a voucher from another site.
You select a voucher from the OH site. The open payment was entered in the MI site, and is being applied in the MI site. When you select Apply, the entries look like the following:
MI Site
| 35 | * 01/17/2003 | 11600 | 100.00 | APPR | 23 |
| AP Deposit | 100.00 | USD | 1.000 | ||
| 36 | * 01/17/2003 | 49010 | 100.00 | APPR | 23 |
| A/P Inter-Site Asset | 100.00 | USD | 1.000 |
OH Site
| 47 | * 01/17/2003 | 20000 | 100.00 | APPR | 23 |
| Accounts Payable | 100.00 | USD | 1.000 | ||
| 48 | * 01/17/2003 | 49030 | 100.00 | APPR | 23 |
| A/P Inter-Site Liability | 100.00 | USD | 1.000 |
Reapplying an open payment to a voucher with a different exchange rate.
You apply an open payment for $310 Canadian Dollars (CND, at an exchange rate of 1.55) to a voucher with an exchange rate of 1.60. The following entries display in the journal when you select Apply:
| 66 | * 01/14/2003 | 11600 | 200.00 | APPR | 5651 |
| AP Deposit | 310.00 | USD | 1.550 | ||
| 67 | * 01/14/2003 | 50600 | 7.03 | APX | |
| Currency Loss | 10.90 | CND | 1.550 | ||
| 68 | * 01/14/2003 | 20000 | 7.03 | APX | |
| Accounts Payable | 10.90 | CND | 1.550 | ||
| 69 | * 01/14/2003 | 20000 | 200.00 | APPR | 5651 |
| Accounts Payable | 310.00 | CND | 1.550 |
You enter a payment for $75 with a non-A/P distribution of $5. You open the A/P Quick Payment Application form, and select the Open and Voucher records. The transactions now display as follows:
| Type | Voucher | Site | PO | Check | Invoice Date | Due Date | Amt to Pay | Discount |
|---|---|---|---|---|---|---|---|---|
| Non-A/P | 01 | 05/15/2002 | 5.00 | 0.00 | ||||
| Open | 01 | 1 | 05/15/2002 | 20.00 | 0.00 | |||
| Voucher | 100 | 01 | 05/15/2002 | 06/15/2002 | 90.00 | 0.00 |
You first apply the $20 open payment to the voucher. The system then creates distributions for $5.00 for Non-A/P cash, and a $70.00 voucher. The Non-A/P cash should already exist in the distributions, so the system will delete and recreate it.
Using A/P Quick Payment Application to Enter and Apply Full and Partial Payments
Using A/P Quick Payment Application to Reapply Open Payments
Using the A/P Quick Payment Application to Enter and Distribute an Open Payment