Currency Revaluation Utility
Use the Currency Revaluation Utility to generate realized 
 or unrealized currency gains and losses (due to currency rate changes) 
 for these accounts:
	- open payable
- vouchers payable
- receivable
NOTE: This utility 
 should be run prior to creating financial statements.
You can run this utility with or without posting to 
 the respective A/P, PO, or A/R distribution journals. When generating 
 realized gains and losses, the utility includes gain/loss amounts previously 
 posted to the A/P and A/R journals.
Posting realized gains and losses rewrites historical 
 rates in the open transactions. Posting unrealized gains and losses creates 
 the journal entries as reversing entries.
The results grid for the Currency Revaluation Utility 
 includes the following information:
	- Customer number and name
- Invoice number
- Vendor number and name
- Currency
- PO
- Invoice/Voucher number
- Detail Description
- Exchange Rate
- Foreign Total Amount -
The Foreign Total Amount is the foreign currency transaction amount. 
The Old Amount is the domestic currency amount converted from the Foreign 
 Total Amount using the old exchange rate (the exchange rate on the transaction 
 prior to revaluing). 
The New Amount is the domestic currency amount converted from the Foreign 
 Total Amount using the revalued exchange rate. 
The Cost of Revaluation is the gain or loss amount associated with that 
 particular transaction. 
The Gain or Loss Amount is the currency gain/loss amount generated for 
 the particular invoice or voucher (total of all associated "Cost 
 of Revaluation" amounts for that invoice or voucher).
	- Account number
- Account Unit 1-4 reporting units
- Domestic Total Amount Debit 1-2
- Domestic Total Amount Credit 1-2
- Net Loss
- Net Gain
- Variance Account number
- Variance Account 1-4
- Description - This field is in 
	 the grid twice. One is the description of the Account number. The 
	 other is the description of Variance Account number.
Related Topics
Using 
 Utilities and Activities
About 
 Realized and Unrealized Gains and Losses