A/R Posting

Use the A/R Posting forms (A/R Payment Posting, A/R Wire Posting, A/R Draft Posting, or A/R Adjustment Posting) to post payments and distribution transactions to Open Item, Customer and G/L Journal records. You should perform the posting after reviewing all payment transactions and their distribution records that you have on hand.

When posting multiple checks, wires, and adjustments, a summary entry is created on the Bank Reconciliations form. You can also post checks, wires, and adjustments individually to create individual bank reconciliation entries.

When you select one of the posting forms, the system verifies that the A/R account is defined. Therefore, you must define the default A/R account even if the payment you are posting does not post to this account. This action prevents you from posting blank account numbers to the journals (an error message displays if the default A/R account is not defined).

For A/R Payment posting, if there are records that contain deposit dates, the system will use those dates as the journal posting date; otherwise, the system will use the receipt date. If the deposit date is later than the site's system date, records with those deposit dates will not be posted.

On the Order Entry Parameters form, if the Commission Due on Payment system parameter is selected, each time you post payments to a customer, the system scans the open items for fully paid invoices. Then, the system updates the corresponding commission due record with the new commission amount.


Related Topics

About A/R Posting

Accounts Receivable Steps

Posting A/R Draft Payments

Posting Payments

Using Utilities and Activities

About Realized and Unrealized Gains and Losses