Rebalance Ledger Period Totals

Use the Rebalance Ledger Period Totals utility to create period total records that contain the sum of the transactions for a particular period.

Creating period totals improves the speed with which reports can run, because the system calculates account balances at the time the report is printed. It does not store totals. To get a total, it must sum up ledger transactions for an account up through the required date.

When calculating a balance, the system first sums up the period total records that apply, and then adds in the ledger transactions that close the gap between the end of an accounting period and the requested date.

EXAMPLE: You may request an account balance on 4/15, but the accounting periods end on 3/31 and 4/30. The system sums up period total records through 3/31 and ledger transactions from 4/1 through 4/15 to arrive at the total.

This utility processes all ledger transactions and creates balance totals per period, for each account. This information is then used for General Ledger reporting.

Run this utility if you suspect that the period totals are not correct, because it takes some time if there are a lot of ledger transactions.

You may also want to run this utility when you have sort methods that need to be maintained only for a short period of time.

EXAMPLE: Suppose you have defined a sort method for a financial report that is needed for year end closing. Maintaining this report throughout the year would be an unwanted performance hit for eleven months. You would leave the index inactive for eleven months and when the time came to run your report, you would run this utility for this one sort method and select the Active Only check box. Once you are done with your year end reporting, you would go to the Period Sorting Methods form and deactivate the sort method until next year.

When you run this utility, the Index Active check box for each sort method in the specified range is not selected, preventing other programs that are run by other users from looking at these period total records and retrieving a potentially incorrect or partial amount. When the utility completes successfully, the Index Active check box is then selected.

NOTE: If the utility does not run to completion (because, for example, of a power outage or system failure), the Index Active check box will not be selected, and the account balance calculation will be slow because the system cannot reliably look at period totals. Re-run this utility, and do not select the Active Only check box.


Related Topics

Troubleshooting Financial Statements

Using Utilities and Activities