Journal Resequencing

Use the Journal Resequencing form to change the sequence numbers for the journal transactions. Resequencing does not change the order of the transactions; it changes only the sequence numbers. A range of sequence numbers can also be changed.

EXAMPLE: You can change 1, 2, 5, 10 to 10, 20, 30, 40.

You need to resequence a journal after adding a new transaction that falls between two consecutive transactions.

Resetting Sequence Numbers

On the Journal Entries form, select Actions > Sequence Reset. The Journal Resequencing form displays. When you enter the sequence values and select Process, the system checks to see if the values will generate a valid resequencing. If so, it performs the resequencing.


Related Topics