External Financial Interface Data Request Utility
Certain types of financial data may be maintained 
 only in an external financial system. However, SyteLine 
 may need access to some of that data for its production or customer service 
 activities.
Use this utility to submit requests to an external 
 financial interface for certain types of information (chart of accounts, 
 tax codes, and so on). The requests are processed as background tasks 
 that build XML LoadCollection requests, which are then sent using non-transactional 
 replication to the external financial system. The external financial system 
 responds with UpdateCollection XML requests that update SyteLine tables with 
 data from the external financial system.
You can run this utility manually (by clicking the 
 Process button) or as a background 
 process run on a regular basis.
	NOTES:
	
		- This utility is not used when running the SyteLine Enterprise 
		 Financials package that works with Infor SunSystems.
- Before using this utility, you must set up the external financial 
		 interface as described in Updating 
		 SyteLine 
		 Data from Data in an External Financial Application.
- The data request utility is available only if you have selected 
		 Use External Financial Interface on 
		 the External 
		 Financial Interface Parameters form. This utility is 
		 needed only if the external system does not have the ability to 
		 "push" its data to SyteLine.
- If records have been deleted in the external system, the corresponding 
		 records must be deleted manually in SyteLine. 
		 This utility does not delete records.
- For Infor Global Financials (IGF) integration, only Chart 
		 of Accounts, Currency 
		 Codes, and Currency Rates 
		 can be selected on the Table tab. All fields are available for 
		 use on the Customer Posted Balance tab. The IGF integration uses 
		 direct data access with this utility to retrieve data for SyteLine.
 
The Customer Posted Balance tab is enabled only if 
 the Use External A/R System field is selected on the External 
 Financial Interface Parameters form.
Related Topics
Handling 
 Replication Data and Communication Errors
Updating 
 SyteLine Data from Data in an External Financial Application
Setting 
 Up an External Financial Interface