About Unit Code Implementation

Due to a change in unit code functionality beginning with SyteLine 6.0, you may need to perform the following procedure if you upgrade from version SyteLine 6.0 or earlier to SyteLine 7.0 or later.

NOTE: Beginning with SyteLine 6.0, unit codes can be marked as Required on the Chart of Accounts form.

Change Existing Accounts

  1. Upgrade to SyteLine 7.0 or later.

    All unit codes marked as not accessible are assigned a status of Not Accessible. All unit codes marked as accessible are assigned a status of Accessible.

  2. If you want to change unit code status to Required on the Chart of Accounts form, post to journals first. If you do not, a warning message tells you to post before you change the status.
  3. Run the Unit Code Where Used Report.

    This report identifies areas in the system where a particular unit code is referenced.

  4. Make corrections in the areas of the system where the Unit Code Where Used Report indicated that a unit code should be filled in for the account.

Related Topics

Account/Unit Code Removal Utility

Copy Unit Codes to Accounts Utility

Unit Code Replacement Utility