Fixed Assets Overview
What Are Fixed Assets?
Fixed assets are items a company
owns and uses in its operation. Fixed assets do not include assets used
for resale purposes, such as inventory, and those held on a temporary
or short-term basis. Examples of fixed assets include:
- Equipment
- Furniture and fixtures
- Buildings
- Leasehold improvements
What Is Depreciation?
You do not usually expense fixed assets during the year you acquire
them. Rather, you record their value as an asset on the balance sheet
and depreciate the value over their useful life.
Fixed assets can accommodate many types of depreciation methods. SyteLine provides seven
predefined depreciation methods and allows you to add additional, custom
depreciation methods. You can also maintain up to four separate depreciation
schedules for each fixed asset. This feature allows you to maintain both
your book and tax records on one system.
Several factors influence the method selected for calculating fixed
asset depreciation:
- The expected useful life of the asset
- The expected salvage value at the end of its useful life
- Its original cost
After the system calculates depreciation for a particular accounting
period, it records the depreciation onto the General Ledger as a debit
to the depreciation expense and as a credit to the accumulated depreciation.
Fixed Assets and the General Ledger
Fixed Assets operate with the General Ledger in the following ways:
- During Fixed Assets Disposal, the system credits the asset account
and debits the Accumulated Depreciation account. (You enter any remaining
distributions manually.)
- During Fixed Assets Transfer, when transferring from one Class
Code to another, the system transfers the asset from the old asset
account (and its accumulated depreciation account) to the new asset
account and its accumulated depreciation account.
- During depreciation posting (for the BOOK schedule only), the system
posts to the Depreciation Expense account and to the Accumulated Depreciation
account.
- When you enter a Fixed Assets purchase, you must enter an acquisition
transaction into the General Ledger to debit the Asset account and
credit the Cash account.
- Fixed Asset records are created when the Fixed Asset Number is
assigned on the Purchase Order Line.
- Any line received with a Fixed Asset number updates the Fixed Asset
Acquired date.
Related Topics
Fixed Assets Steps