Creating Open Payments for a Customer
To enter a payment that is applied to the customer's total account balance,
use the following procedure. This type of payment is the only payment
type required for balance forward customers. For open item customers,
these open credits need to be reapplied against invoices or finance charges
at a future time.
- On the A/R
Payments form, select Actions > New.
- Enter the appropriate information in the following fields:
- Customer - Select the number
of the customer the payment is for.
- Type - This field displays
the customer's default payment method, but you can select a different
method.
- Number - Enter the check
or draft number of the payment.
- Receipt Date - Enter the
date you received the payment, or accept the default, which is
today's date.
- Payment Due Date - (Available
only if the payment type is Draft.) Enter the date the
draft is due.
- G/L Reference - Enter a description
to appear in the distribution journal for this transaction, or
accept the default, which is ARP, followed by the check
or draft number.
- Description - Enter a description
to appear in the distribution journal for this transaction, or
accept the default description.
- Bank Code - The customer's
default bank code displays, but you can select a different code
of the bank into which the payment will be deposited.
- Customer Amount - Enter the
amount of the payment.
- Select Actions > Save.
- To distribute the payment, using the A/R
Payment Distributions form, click Distributions.
- Under the General tab, in the Type field, select
Open Credit.
- In the Order field, enter the number of the sales order
to which the payment is to be applied.
- In the Dist Amount field, enter the amount to apply against
the customer's sales order or the amount to post as an open payment.
- In the Disc/Credit 1 and Allowance/Credit 2 fields,
enter the discount and allowance, if applicable.
- Select Actions > Save.
Related Topics
Accounts
Receivable Steps