Distributing Invoices
You can distribute invoice amounts to multiple General Ledger (G/L)
accounts, using any of three methods:
Automatic Distribution
- On the Invoices,
Debit and Credit Memos or Invoices,
Debit and Credit Memos G/L Distribution form, select the record
for the invoice you want to distribute.
- Select Actions > Generate Distributions.
NOTE: The default
G/L accounts from the Accounts Receivable Parameters form and the
customer's tax code are used.
Manual Distribution
- On the Invoices, Debit and Credit Memos G/L Distribution
form, select Actions > New.
- Select the customer for which you are adding a distribution.
- Select the number of the invoice you are distributing.
- In the Dist Seq field, accept the default, which is the
next available sequence number.
This number is used to order the distributions.
- In the Tax System field, select the tax system for the distribution;
or, for a non-tax distribution, leave this field blank.
- In the Dist Amount field, enter the amount of the distribution.
- In the Account field, select the account to post the distribution
to.
- Select Actions > Save.
- To continue adding distributions until the Total Remaining
field is 0 (zero), repeat these steps as necessary.
Reapplication of an Open
Credit
- On the A/R
Posted Transactions Detail form, locate the open credit you
want to reapply.
- Make a note of the customer, debit or credit transaction, check/reference
number, and invoice number associated with the transaction.
- Follow the remaining steps in the topic Reapplying
Open Payments.
Related Topics
Accounts
Receivable Steps