Distributing Vendor Payments Manually
To distribute vendor payments manually:
- On the A/P
Payment Distributions form, select Actions > New.
- In the Vendor field, select the vendor from the list of
those with payments on file.
The payment header information displays in the upper part of the
form, and you cannot change it.
- On the General tab, fill in the required data:
- Type - Select the distribution
type: Voucher, Non A/P, Commission or Open.
- Vch/Seq - If you are adding
a voucher distribution, enter the number of the voucher referenced
from the distribution. If you are entering any other type of distribution,
enter its sequence number. The sequence number is used only to
keep the distributions in numerical order.
- Site - If the distribution
type is Non A/P, Commission, or Open, select
the site where the transaction resides. If the distribution type
is Voucher, the site that contains the posted transaction
against which the payment distribution is being applied displays
for reference.
- Invoice - If the distribution
type is Non A/P, Commission, or Open, enter
the number of the invoice you are applying the distribution against.
For a Commission distribution type, you must enter an order
entry invoice number with a commission type of Distribution;
the sum of the commissions for that invoice and vendor displays
in the Amount Paid field on the Accounts tab.
- PO - If the distribution
type is Non A/P, Commission, or Open, enter
the PO number to which you want to record the payment.
- 1099 Reportable - If
the payment distribution is 1099 taxable and should be included
on the vendor's 1099 form, this check box should be selected.
If the payment is not 1099 taxable, clear the check box.
- Select the Accounts tab, and then fill in data in the following
fields:
- Amount Paid - Enter the amount
to apply to this payment.
- Disc Taken - If the payment
type is Voucher, enter the amount to be discounted from
this payment.
- [Tax Adjustment (1)] - If
the payment type is Voucher, this field displays any Tax
System 1 adjustment for discounts. You can change this amount.
- [Tax Adjustment (2)] - If
the payment type is Voucher and a second tax system is
defined, this field displays any Tax System 2 adjustment for discounts.
You can change this amount.
- Disc Account - If the payment
type is:
- Voucher, this field displays
the discount account number from the Accounts
Payable Parameters form. If the discount amount is
not zero, you can select a different account for the discount
amount, if applicable.
- Non A/P, select the number
of the General Ledger account that is to receive the distribution
amount. This account offsets the cash account.
- Commission, this field
displays the number of the General Ledger commission paid
account from the Accounts
Payable Parameters form, but you can select a different
account to apply the payment to.
- Open, this field displays
the number of the General Ledger deposit account from the
Accounts
Payable Parameters form, but you can select a different
account to apply the payment to.
- To save the distribution, select Actions > Save.
NOTE: Distributions
of type Non-A/P or Commission are not permitted for payments
where the Payment
Type is Standard Draft.
Related Topics
Accounts Payable
Steps
Posting Vouchers
- Detail