Maintaining the Multi-FSB Chart of Accounts

Use the Multi-FSB Chart of Accounts form to manually set up and maintain mapping of multi-FSB accounts with accounts from the standard GL Chart of Accounts.

NOTE: You can initially map multi-FSB accounts automatically by copying the standard GL Chart of Accounts using the Copy COA button on the Multi-FSB Charts form. Then use this form to add, remove, or change account mapping.

To map an account:
  1. Open the Multi-FSB Chart of Accounts form.
  2. Select Actions > New.
  3. In the FSB COA field, select a multi-FSB chart of accounts to work with.
  4. In the FSB Account field, specify an identifier for the multi-FSB account.
  5. In the field to the right of the FSB Account field, specify a description of the account for reference.
  6. In the FSB Account Type field, select the account type.
  7. Optionally, you can specify an FSB Account Class for financial reporting.
  8. Do one of the following:
  9. On the associated Unit Code tabs, you can add or remove unit codes.

  10.   To save the account mapping, select Actions > Save.

Related Topics

Multiple Financial Sets of Books Overview