Printing a Financial Statement
NOTE: Before you
can print a financial statement, you must have first set up it up and
defined its columns and lines. For more information, see the Financial Statement Setup
Help topic.
- Open the Financial
Statement Output form.
- Perform one of the following actions:
- To produce a single report, in the Report ID field,
select the ID of the report you want to print.
- To produce a group of reports, select Actions > Get Group,
select the group number of the reports, and select OK.
The system updates the Financial Statement Output form with
all the reports in that group, and you can define each one's output
parameters.
- Select the check box for each type of detail you want to include
in the financial statement.
- In the Report Type drop-down list, select the type of report
you want to run.
- In the Currency drop-down list, select the currency to use.
By default, the system produces the report in your domestic currency,
but you can change it to a different currency.
- In the Current Date field, select the effective date for
the report. By default, the system uses the current system date, but
you can change it to a different date.
- In the Site Group field, select the site you want to produce
the report for, or, to produce the report for all sites, select All.
- From the Line Summary Level drop-down list, select the desired
level of output detail for the report:
- Direct Reports - Displays
one line for each account and for each site. If the direct report
is an entity, it reports to the current entity and then summarizes
all sites for that entity into a single line.
- Site - Displays one line
for each account and for each site.
- Summary - Displays and summarizes
all sites into a single line for each account. Your selection
in the Site Group field determines which sites to include.
If this is an entity, the report displays all sites that report
to the entity.
- You can overwrite the following report definition settings for
the purpose of this print run:
- Year Start
- Period
- Period Start and Period
End
- From Unit Code 1-4 and To
Unit Code 1-4
- Sort Order
- Select Print.
Related Topics