Printing and Posting Vouchers

To print and post vouchers:

  1. If your company uses the Voucher Authorization feature, run the Voucher Authorization utility before posting the approved transactions.

    NOTE: Running the Voucher Authorization utility is not required before posting transactions. The posting process allows you to post vouchers with authorization statuses of Approved and/or Matched.

  2. On the A/P Voucher Posting form, provide information in the following fields:
  3. To print and review the A/P Voucher Posting report, select Print.
  4. When you are ready to post the vouchers, select Commit and then click Process.

You can view the posted vouchers using the A/P Posted Transactions Detail and A/P Posted Transactions Summary forms.

NOTE: If you use the External Financial Interface, additional processing may occur during voucher posting. For more information, see "Setting Up an External Financial Interface."


Related Topics

Accounts Payable Steps

Posting Vouchers - Detail