Setting Up Electronic Funds Transfer for A/P

Electronic funds transfer (EFT) is a common way to process automatic transfer of funds from a company's bank account to its vendors. SyteLine supports various output file formats for submission to third-party EFT transmission systems.

To set up EFT:

  1. On the Bank Codes form, specify information about the bank that you will use for EFT transactions. For SEPA format only, specify the business identifier code (BIC) and international bank account number (IBAN).
  2. On the Accounts Payable Parameters form, set up the EFT parameters for:

    After EFT processing has begun, this tab also shows the last date an EFT file was created, and the name (number) of that file.

  3. In the Remittance Advice area to the right of the EFT parameters, indicate whether you want to print remittance advice after posting EFT transactions.
  4. On the Vendors or Multi-Site Vendors form, set up EFT information for the individual vendors. If the vendor's default payment type is EFT, enter the following information (depending on the EFT format you use):

For posting steps, see Posting Electronic Funds Transfer Transactions.


Related Topics

A/P EFT Posting

Accounts Payable Steps

EFT Output Files

Posting Electronic Funds Transfer Transactions