Voiding Posted Drafts

After posting drafts, you can void them, using either the A/P Payments form or the Void Posted Draft Payments form.

After voiding the drafts, you may reprint them.

Voiding Drafts Using the A/P Payments Form

To void drafts using the A/P Payments form:

  1. Select Actions > New.
  2. Enter the following required information:
  3. Enter the following information only for incoming drafts:
  4. (Optional) In the G/L Reference field, enter a description for this transaction that is to appear in the journals.

    The default is APP, followed by the vendor number.

  5. Save the record.
  6. Select Distributions.
  7. Select Actions > New.
  8. Distribute to the vouchers as a negative amount.
  9. Print and post the draft.

Voiding Drafts Using the Void Posted Draft Payment Utility

NOTE: If the A/P payments are standard drafts, are compressed, or are multi-site, you cannot void them using this utility.

To void drafts using the Void Posted Draft Payments form:

  1. Enter data in the following fields:
  2. Perform one of the following actions:
  3. Select Process.

Related Topics

Accounts Payable Steps

Printing and Posting A/P Drafts