This field applies to APS and the Scheduler. MRP uses this value indirectly, along with the other operation times, if you use the Lead Time Processor to calculate lead times.
Enter the delay in hours between completion of this operation and the start of the next one in the routing. On the Operations forms, this value defaults from the work center record.
For example, this delay could represent time an item needs to be idle (such as cooling time) before proceeding to the next operation. During this period, the delayed load of items does not utilize the resources used at this operation or at the subsequent operation.
Between two operations, if a Move value and a Finish value are both specified, the system adds the two values together.
If an item is assembled into another item, the system uses the Finish value for the last operation of the component item and the Move value for the first operation of the item being assembled.