Infinite Planning

This field applies to APS when running in finite mode.

Select the field to define this resource as having infinite capacity. Infinite Planning resources can perform an unlimited number of manufacturing operations simultaneously, but only when on-shift.

NOTE: This value overrides the Infinite Resource Capacity After setting (defined globally on Planning Parameters or for a resource group on the Resource Groups form). For example, if the resource is an Infinite Planning resource, and is a member of a resource group that has Infinite Capacity After 999 hours, this resource is considered infinite. See About Infinite Resource Capacity for more information about ways to represent infinite capacity.