This field applies to APS when running in finite mode.
Enter the number of hours after which the resource can work on an infinite number of operations simultaneously (while on a working shift period, and within the Plan Horizon). For example, if you enter 4, the resource has infinite capacity beginning four hours after the Planning run is started.
On the APS Mode form, you can define this value globally, for all resources.
On the Resource Groups form, you can define this value for all resources in a particular resource group. If the resource group's Infinite Capacity After value is smaller (that is, if it occurs earlier) than the global Planning Mode value, it overrides the global value.
Set the parameter to 0 to make the resource infinite over the entire Plan Horizon (that is, after zero hours). The default setting is 999999, which indicates the resource always has finite capacity.
You can change this field only when the planning mode is APS.
NOTE: To make a single resource infinite, select the Infinite Planning field on the Resources form.