This field applies to APS and the Scheduler. MRP uses this value indirectly, along with the other operation times, if you use the Lead Time Processor to calculate lead times.
Move hours is the amount of time to schedule for movement of WIP inventory from the previous operation to this operation.
This value defaults from the Shop Floor Control Parameters form. If the work center is specified as Outside (on the Work Centers form), the value in the Shop Floor Control Parameters Outside Move field is used. Otherwise, the value in the Shop Floor Control Parameters Move Hours field is used.