Select the type of data entry validation for the system to perform when you enter invalid data for a job transaction.
These validation checks can prevent you from entering incorrect quantities on the following types of transactions, allowing you to correct the errors before posting the transactions:
The validation checks can display the following error messages (values in brackets [] are sample values):
| Message | Description |
|---|---|
| Completed is not equal to [25] for Job Transaction that has [Oper: 10]. | The operation is Complete and the (transaction quantity Completed) does not equal the (job quantity Released) - (operation quantity already Completed) - (total operation quantity Scrapped) - (transaction quantity Scrapped) |
| Completed is greater than [25] for Job Transaction that has [Oper: 10]. | The operation is not Complete and the (transaction quantity Completed) is greater than the (job quantity Released) - (operation quantity already Completed) - (total operation quantity Scrapped) - (transaction quantity Scrapped) |
| Completed is not equal to [25] for Job Transaction that has [Oper: 10]. | This is the last operation and the (transaction quantity Completed) + (operation quantity already Completed) is not equal to (job quantity Released) - (total operation quantity Scrapped) - (transaction quantity Scrapped) |
| Complete? is equal to No for Job Transaction that has [Oper: 10]. | This is the last operation and the (transaction quantity Completed) + (operation quantity already Completed) equals (job quantity Released) - (total operation quantity Scrapped) - (transaction quantity Scrapped) and an earlier operation is not Complete. This message displays only if a prior operation is not complete and is marked as a control point. |
| Qty Issued is not equal to [25] for Job Material that has [Item: FA-10000] and [Oper: 10]. | This message appears if a location is entered for the Operation, and if, for each backflushed job material of each operation, the job material's quantity issued is not equal to its quantity required. |
| Qty Issued is less than [25] for Job Material that has [Item: FA-10000] and [Oper: 10]. | This message appears if a location is entered for the operation, and if, for each NON-backflushed job material of each operation, the job material's Qty Issued is less than its Qty required. |
| Message | Description |
|---|---|
| At least one Job Transaction exists for Job. | An unposted job transaction exists for the job or there is a record for the job in the system DC Error Processing file (dcsfc). |
| Not one Job Transaction exists for Job Operation that has Job: J000000010] and [Job Suffix: 0001] and [Oper: 10]. | There are no posted job transaction records for the last operation of the job. |
| [52] is greater than [25] for Job that has [Job: J000000010-0001]. | For the last operation for the job, (quantity to be received) + (job quantity completed) is greater than (operation quantity completed) |
| [24] is less than [25] for Job that has [Job: J000000010-0001]. | For the last operation for the job, (quantity to be received) + (job quantity completed) is less than (operation quantity complete) |