This field applies to MRP and APS.
When the system is planning released jobs and production schedule releases, this field controls whether the materials for a job or production schedule release are required to be available at the operation's start date or at the job/PS release start date.
NOTES:
When MRP generates a PLN to satisfy a demand, it always plans the materials to be due at the start of the job. For jobs and production schedule releases, MRP considers the Plan Materials at Operation Start field when the following conditions are true:
The table below summarizes the other factors that determine how MRP plans the due date of materials:
| Job Scheduled AND Use Scheduled Times in Planning selected? | Job Start Date | Materials are due at |
|---|---|---|
| No | Not blank | Job's Start date |
| No | Blank | Job's End date - Fixed Lead Time + (Variable Lead Time * Qty) |
| Yes | n/a | Job's internal projected start date (calculated by the Scheduler--not displayed elsewhere) |
| Job Scheduled AND Use Scheduled Times in Planning selected? | Operation Start Date | Job Start Date | Materials are due at |
|---|---|---|---|
| Yes | Not blank | n/a | Operation Start Date |
| Yes | Blank | n/a | Job's internal projected start date (calculated by the Scheduler--not displayed elsewhere) |
| No | n/a | Not blank | Job Start Date |
| No | n/a | Blank | Job's End date - Fixed Lead Time + (Variable Lead Time * Qty) |
If the job or production schedule is released but NOT scheduled, APS plans the materials based on the setting of the Plan Materials at Operation Start field.
NOTES: These notes apply if you are using APS.