Select a rule to determine how an arriving job affects the quantity for a forming batch load, that is, when a batch will be released to be processed. This rule is used in conjunction with the Value, Minimum, and Maximum fields. For example, if you select One per Job with a Minimum of 3, then whenever 3 jobs arrive and are ready for processing, a batch is created and begins processing through the batch definition routing.
| Rule | Description |
|---|---|
| One Per Job | Count one per job. |
| One per Item | Count the quantity in the job. |
| Attribute Value | Count based on the batching release attributes specified for each item on the Items form. These release attributes (Release 1, Release 2, Release 3) are multiplied together (for those greater than zero) to determine how much this job or production schedule will contribute to the batch. |
| Constant Value | Count based on the number in the Value field. |
| User-Defined Release Rules | Count according to a user-defined rule. For more information, see Writing Custom Batch Release Rules. |