Required Quantity

The required quantity displays. This field is calculated differently depending on the type of replenishment method you used when you ran the Material Planner Workbench Generation:

You can change the value in this field as desired. You can use this field to combine requirements into one planned order. Be sure to remove any unnecessary lines after you have combined the quantities. To do this, set the required quantity to zero, then process the record. When you process a zero-quantity record, it is deleted from the system.