Selecting this field may improve the accuracy of the plan for manufactured items with safety stock defined. After the first planner logic phase is complete, the system determines manufactured item safety stock requirements. These requirements are added to the original requirements, and then a second planner logic phase occurs.
If the Days Supply Planning field is selected, this field is automatically selected and disabled.
Note: Selecting this field can significantly increase the amount of time it takes for the APS Planner to run.