Transaction Description

The system derives this description from information in the Transaction Type, Ref Type, and Quantity fields. The code simply provides more information about the material transaction. The drop-down list allows you to filter on all transactions of a given type.

NOTE: You can filter only on the types of transactions that have been posted. Only those transaction types currently present in the material transactions database table are displayed in the drop-down list.

The table below lists the possible transaction descriptions and how they were derived:

Transaction Description displays this value if... Transaction Type is and Reference Type is and Quantity is
A Stock Adjust Adjustment n/a <> 0
AC Cost Adjust Adjustment n/a 0
B Cycle Count Cycle Count n/a n/a
CS Job Split Split/Merge/Create n/a < 0
CM Job Merge Split/Merge/Create n/a >= 0
CA JIT WIP Created Split/Merge/Create JIT Production n/a
CB PS Wip Created Split/Merge/Create Production Schedule n/a
C Job WIP Created Split/Merge/Create n/a n/a
DA PS Scrap Return Scrap n/a < 0
DS PS Scrap Issue Scrap n/a >= 0
FK JIT Finish Finish JIT Production n/a
FS PS Finish Finish Production Schedule n/a
F Job Finish Finish n/a n/a
G Misc Issue Misc Issue n/a n/a
H Misc Rcpt Misc Receipt n/a n/a
IC Project Resource Issue Issue/WIP Change Project n/a
CK JIT WIP Change Issue/WIP Change JIT Production = 0
IK JIT Issue Issue/WIP Change JIT Production <> 0
CP PS WIP Change Issue/WIP Change Production Schedule = 0
IS PS Issue Issue/WIP Change Production Schedule <> 0
IW MC Matl Issue Issue/WIP Change Work Center n/a
CF Job WIP Change Issue/WIP Change n/a = 0
I Job Issue Issue/WIP Change n/a <> 0
L Transfer Loss Transfer Loss n/a n/a
MT Stock Move To Stock Move n/a > 0
M Stock Move From Stock Move n/a <= 0
NK JIT Labor Labor Next Operation JIT Production = 0
NA JIT Next Oper Labor Next Operation JIT Production <> 0
NS PS Labor Labor Next Operation Production Schedule = 0
NB PS Next Oper Labor Next Operation Production Schedule <> 0
NW WC Labor Labor Next Operation Work Center n/a
NL Job Labor Labor Next Operation n/a = 0
N Job Next Oper Labor Next Operation n/a <> 0
OW WC Other Cost Other Cost Work Center n/a
O Job Other Cost Other Cost n/a n/a
P Physical Invent Physical Inventory n/a n/a
RK JIT Receipt Receipt JIT Production n/a
RS PS Receipt Receipt Production Schedule n/a
RA PO Receipt Adj Receipt n/a < 0
R PO Receipt Receipt n/a > 0
V PO Cost Varianc Receipt n/a = 0
SA CO Ship Adj Ship n/a > 0
S CO Shipment Ship n/a <= 0
TT Transfer To Transfer n/a > 0
T Transfer From Transfer n/a <= 0
WC Project Resource Return Withdrawal/Return Project n/a
W Job Withdrawal Withdrawal/Return Job n/a
WK JIT Return Withdrawal/Return JIT Production n/a
WO CO Return Withdrawal/Return Customer Order > 0
WA CO Return Adj Withdrawal/Return Customer Order <= 0
WM RMA Return Withdrawal/Return RMA n/a
WR PO Return Adj Withdrawal/Return Purchase Order > 0
WP PO Return Withdrawal/Return Purchase Order >= 0
WS PS Return Withdrawal/Return Production Schedule n/a
WW WC Matl Return Withdrawal/Return Work Center n/a