Item Stockroom Locations

Use this form to create a record of every location where an item is to be kept. You can maintain the lot number and quantity-on-hand for each location of each item. Also, you can specify nettable and non-nettable locations and to view detailed information when more than one location is used for each item, including an item's quantity, location, and the quantity available at the location.

NOTE: Non-nettable stock locations are not available for selection when moving inventory to a production line. Scrapped inventory is moved to non-nettable stock locations.

When you move or adjust a quantity or add a new location, a material transaction is created to provide an audit trail. You may print this audit trail with the Material Transaction Report. Material transactions are also created when you:

Accounting Considerations

When you create a new stockroom location, the system creates records in the Inventory Control Ledger Distribution Journal in the General Ledger. For either Actual or Standard costing (specified in the Inventory Parameters), the transaction is posted only if a quantity is entered for the location at the same time it is added. The amount used is the quantity entered multiplied by the unit cost. For Actual costing, the unit cost used depends on the cost flow method specified for the item. For Standard costing, the standard unit cost is used.

The Update function creates records in the Inventory Control Ledger Distribution Journal in the General Ledger. For either Actual or Standard costing (specified in the Inventory Parameters), the transaction is created only if the inventory account tied to the location is changed. When using the Specific cost flow method, a transaction is also created when the unit cost tied to a location is changed.

Auto-Delete of Item Stockroom Locations

The Permanent check box identifies a location as permanent or temporary. If the location is temporary, the item stockroom location is automatically deleted when the On Hand quantity becomes zero through any of the following transactions:


Related Topics

Creating Item Stockroom Locations When Entering Transactions