Standard Materials

The system uses the Standard Materials and Standard Operations forms for costing purposes.

Use the Roll Current Cost to Standard Cost utility for items using Standard costing. This utility copies the information on the Current Materials form to the Standard Materials form. You usually run the Roll Current Cost to Standard Cost utility periodically, such as once a year.

When you set the Calculate Variances Against field to Standard on the General Parameters form, the system uses Standard costs for calculating variances and report costing.

NOTE: You can update the Current Materials form at any time without affecting its Standard counterpart. The system updates the Standard Materials form only if you rerun the Roll Current Cost to Standard Cost utility.

Costs Tab

Use the Roll Current Cost to Standard Cost utility for items using Standard costing. You usually perform this function periodically, such as once a year.

This utility copies the information on the Current Material Costs form to the Standard Materials Costs tab. Throughout the remainder of the period, the system uses the Standard information (displayed on the Standard Materials Costs tab) for calculating variances and reporting costing. The system uses the Current Materials and Current Operations forms for costing purposes only.

NOTE: You can update the Current Materials Costs tab at any time without affecting its Standard counterpart. The system only updates the Standard Materials Costs tab if you rerun the Roll Current to Standard Utility.

When copying to a job, a production schedule, or an estimate, you must use the Current Materials and Current Operations forms as the template.

NOTE: All fields on the Standard Materials Costs tab default from the Current Materials Costs tab when you perform the Roll Current Cost to Standard Cost utility.

Materials Tab

All of the fields on the Materials tab default from the Current Materials - Materials tab when you perform the Roll Current Cost to Standard Cost utility.

References Tab

Use the References tab to maintain information about each material. This information is for reference purposes. This tab allows you to enter one record for each quantity listed on the Standard Material References tab. For example, if you enter a quantity of four, enter four reference records.


Related Topics