Use the Unit of Measure Conversions form to maintain valid mathematical relationships between units of measure defined on the Unit of Measure Codes form. You can set these conversions to apply at the Global, Item, Item/Customer, or Item/Vendor level.
The Unit of Measure conversion logic is consistent throughout the system. The same conversion factor is used when converting from a base unit of measure to a different unit of measure.
CAUTION: We recommend you do unit of measure maintenance when no other user is running reports, viewing screens, or adding records which would require the unit of measure factors associated with the same unit of measure codes on the records being maintained.
Creating units of measure and unit of measure conversion records