Use the Warehouse to Warehouse Bulk Transfer utility to perform bulk transfer of items in one warehouse to a different warehouse within a site. When you click Process, items are moved from the location in the old warehouse to the location in the new warehouse. Lot tracked and serial tracked items are also moved.
The To Warehouse and the From Warehouse must both exist within the same site. (This control prevents a site from erroneously making a bulk transfer for another site.) This utility does NOT work for bulk transfers where the warehouses are in two different sites.
The old locations still exist after a Bulk Transfer, but the quantity on hand at these locations is zero. If any location does not exist in the new warehouse, the system creates it automatically.
It is possible to have multiple lines per item due to multiple lots and/or multiple LIFO entries along with Actual Costing (LIFO, FIFO, Specific). Unit cost is based on the official G/L cost. Actual Costs, when different, are not shown in the output from this utility. The output is ordered by From Location, item, and lot.
NOTE: This utility will not transfer quantities that are reserved for customer orders.