Backflush Serials Tab

NOTE: This tab is enabled only if the Backflush Serial Numbers option is selected on the Inventory Parameters form, Control tab.

The Backflush Serials tab allows you to select serial-tracked items for inclusion in a backflushing operation.

To generate a list of potential serial-tracked items, click Generate Serials. Then, from the list that is returned, select the items to include in the backflush.

NOTE: If the items are both lot-tracked and serial-tracked, and the grid on the Backflush Lots tab is populated, this tab is disabled until the Target Qty equals the Selected Qty on the Backflush Lots tab.


Related Topics

About Backflushing