The Material Availability Report calculates a rough estimate of how much time is required to manufacture an item, based on current material availability. The report is based solely on a given item and quantity, or on an existing job or estimate job.
Use this report only for rough estimating purposes. To provide relatively quick processing times, the system makes several assumptions:
NOTES: When you run the Material Availability Report for a job, the component quantity issued, but not yet used, counts toward the quantity of the material available.
This report uses the MDAY calendar. See Defining the Work Week for a description of how the MDAY calendar is used
If a shortage of an item exists, this report shows only components of the item. If enough quantity of an item exists, only one line displays.
The availability status displays as the quantity required, quantity available, and date required. If availability for the date required is different than availability for the current date, the system considers the date required to be incorrect. The required date is replaced with the following message:
ASAP Date: Not Available...Rerun Report with Required Date = Today
The current quantity on hand minus any allocations determines the quantity availability (with an option to include released jobs and/or POs). If a shortage exists, the amount of the shortage and an order date display.
The order date is based on the date required less the lead time, dock-to-stock time, and paperwork lead-time. In addition, the system accumulates the longest series of dependent lead times and prints the result as the critical path lead time in manufacturing days.
NOTE: This report will not show reserved quantities as available, regardless of the options you select.