The system allows you to track machine time for data collection solutions in two different ways:
Machine transactions prorated with labor are affected by all labor parameters, including:
For example, in multi-job transactions, labor time and machine time are prorated to 50% labor and 50% machine in a job for machine transactions from the Job Transactions form. If a worker is operating two machines, the system prorates to 33% for labor and 33% for each machine.
Machine transactions independent of labor provide tracking of specific machine transactions for more accurate costing figures.
Machine transactions tracked independently from labor contain the following attributes:
The system keeps track of a specific machine time when a machine set up or machine run process is interrupted for the same job.
If multiple machines are required by a job and you need to track time for each machine, you may want to create multiple operations and work centers to allow for the tracking of machine time after posting.
EXAMPLE: You have a job operation that requires the setup of a machine. You start the machine setup, but have to end it abruptly. Enter the transactions as follows:
| Machine Trans | Hour | Reason |
|---|---|---|
| Start Set Up (F) | 8:00 a.m. | Job setup |
| End Set Up (G) | 8:15 a.m. | Job setup interrupted |
| Start Set Up (H) | 8:30 a.m. | Job setup resumed |
| End Set Up (I) | 9:00 a.m. | Ready to run the job |
If machine setup and run transactions cross midnight, the system automatically generates the end transaction for that day and start transaction for the next day for the same transaction type and machine.
EXAMPLE: Machine setup started at 7:00 p.m. on 3/18 and ended at 3:00 a.m. on 3/19. The machine run started at 3:10 a.m. on 3/19 and ended at 2:00 p.m. on 3/21. The system automatically enters the other transactions (which are shown in bold).
| Machine Trans | Start Time | End Time | Date |
|---|---|---|---|
| Start Set Up | 19:00:00 | 03/18 | |
| End Set Up | 23:59:59 | 03/18 | |
| Start Set Up | 00:00:00 | 03/19 | |
| End Set Up | 03:00:00 | 03/19 | |
| Start Mach Run | 03:10:00 | 03/19 | |
| End Mach Run | 23:59:59 | 03/19 | |
| Start Mach Run | 00:00:00 | 03/20 | |
| End Mach Run | 23:59:59 | 03/20 | |
| Start Mach Run | 00:00:00 | 03/21 | |
| End Mach Run | 14:00:00 | 03/21 |